STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32 cube programmer locks in automatic mode

Automatic mode works fine just to download binaries to the MCU.If It try to set option bytes read out protection to BB afterwards, the software will lock.It displays:15:20:13 : UPLOADING OPTION BYTES DATA ...15:20:13 : Bank : 0x0015:20:13 : Address :...

Alex. M by Associate
  • 3754 Views
  • 5 replies
  • 1 kudos

[Feature Request] Cubeprogrammer address section

Hello,I have a feature request for the STM32CubeProgrammer.As we know, when we connect the board, we can display the memory fields as like following:But when I disconnected from the board, the fields are gone:I know that this is not a bug, its a feat...

mcagriaksoy_0-1711093050768.png mcagriaksoy_1-1711093073833.png mcagriaksoy_2-1711093232799.png

Firmware Upgrade failed CubeProgrammer_API

I am testing firmware upgrade API from CubeProgrammer_API. For some reason, it keeps printing that the firmware upgrade failed, but when i check the firmware version of my device, the firmware has been updated. Does anyone know what is the cause of i...

i124q_0-1710863192582.png
i124q by Associate II
  • 1911 Views
  • 3 replies
  • 0 kudos

Resolved! DFU error using CubeProgrammer_API

I am working on implementing a firmware update on my electron app using CubeProgrammer_API. I keep encountering issues on connecting to the DFU bootloader in which is giving me CUBEPROGRAMMER_ERROR_NOT_SUPPORTED (-5). I compiled my code into a .exe a...

i124q by Associate II
  • 1469 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.