STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! ST-Link-V2 Debugger: No STM32 target found.

Hi :)Problem: STM32F030R8T6 device not found.ErrorMsg in CubeProgrammer: "No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication."ErrorMsg in CubeIde: "Error in initializing ST-LINK d...

STM32CubeProgrammer 2.16.0 DFU Bootloader Error

I am using CubeProgrammer_API to implement a firmware update on my app. I am encountering an error where it cannot connect to the DFU bootloader. The device is visible in device manager and it is properly connected.int usbConnectFlag = connectDfuBoot...

i124q by Associate II
  • 1894 Views
  • 2 replies
  • 0 kudos

Resolved! stlink-gdb-server and Nucleo-H73SL8

While "ST-LINK_gdbserver -d -v --frequency 1000 -cp ..." connects fine to STM32U083C-DK, NUCLEO-H7SL8 does not work.STMicroelectronics ST-LINK GDB server. Version 7.7.0Copyright (c) 2024, STMicroelectronics. All rights reserved.Starting server with t...

Resolved! STM32L051R8 Program Issue with Cube Programmer

I am working with the L051 chip and having issues with the CubeProgrammer Download..History:   we work with many of the STM32 chips.....and have for years, so well versed in this ...so this is an issue that we have not seen using any of the Tools... ...

CTerr.1 by Associate II
  • 3436 Views
  • 6 replies
  • 0 kudos

Connection issue

"My STM32 is locked out of its program. How can I unlock it? I need to continue learning to use it, even though I've just started." STMicroelectronics ST-LINK GDB server. Version 7.5.0Copyright (c) 2023, STMicroelectronics. All rights reserved. Start...

bbb by Associate
  • 1489 Views
  • 2 replies
  • 2 kudos

Resolved! NUCLEO-U575ZI-Q board "Error: No STM32 target found"

Using the STM32CubeProgramer (v2.16 from a Windows 11 laptop) with my NUCLEO-U575ZI-Q board has, from this morning, resulted in only the response:UR connection mode is defined with the HWrst reset modeST-LINK SN : 003E004C3532510F31333430ST-LINK FW :...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.