STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

ST-LINK_gdbserver and load to Ram

It seem that ST-LINK_gdbserver does not implement load to run.(gdb) tar ext :61234 Remote debugging using :61234 0x0800004e in ?? () (gdb) info mem Using memory regions provided by the target. Num Enb Low Addr High Addr Attrs 0 y 0x00000000 0...

Resolved! How to wire stm32c031f6 OTP

HI: I want to write the board SN, REV, TIME to STM32C031F6 OTP area 0x1FFF7000~0x1FFF705F, which is almost 96bytes to write, from the stm32cubeprogrammer manual -W64 command can to write, but is needs to be repeated 6 times, right?Also from the manua...

RJ3 by Associate
  • 1426 Views
  • 2 replies
  • 1 kudos

Resolved! STM32CubeProgrammer

I am trying to program a chip using an STLINK V2. I am using only SWDIO, SWCLK, and ground, and I am powering the chip with 3.3 V. When I try to connect using STM32CubeProgrammer, it does not connect. Am I missing something?

tomm5771 by Associate III
  • 5161 Views
  • 6 replies
  • 1 kudos

Create a dual core project from compiled binary file

Hello,The main purpose of the question is to avoid giving source code and give binary file instead.For example, I generate a compiled binary file from a nucleo project (STM32H743ZI2) for the M7 core.Then I want to create a new dual core project (STM3...

Kévin by Associate III
  • 2216 Views
  • 2 replies
  • 3 kudos

STM32G0 External Loader for I2C eeprom

Hi,I try to make a external loader for STM32G030. I was implemented function MassErase(), Write(), Read(), Init()...First I test function on "flash" version and everything work. But when I try using it in STM32CubeProgrammer the Write function not wo...

arekj by Associate II
  • 2895 Views
  • 4 replies
  • 0 kudos

ST-LINK non recognized on windows 10 and 11

my STLINK is not recognized on Windows (Device description failed). I have try to uninstall and reinstall the driver. I try 3 different ST-Link and different laptop, but I face the same problem. previously, I always used those ST-link on my laptop an...

leli by Associate
  • 2426 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeProgrammer not working

I launched STM32CubeProgrammerIt does not work.It gives me this error message:***CubeProgrammer_API or one of its dependencies is missing.Please try reinstalling the program or check your java architecture.***I reinstalled it.I updated Java on the sy...

FabioCC by Associate II
  • 2658 Views
  • 2 replies
  • 0 kudos

How to write .Bin /.ELF file for External Flash loader

I have a project with a large number of image bitmaps I want to draw to a screen, so have set up an external FLASH IC for storing the majority of these images.I've verified my flash driver works and created an external loader for use in STM32CubeProg...

Alec1 by Associate II
  • 6030 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.