2024-04-21 7:27 PM
HI:
I want to write the board SN, REV, TIME to STM32C031F6 OTP area 0x1FFF7000~0x1FFF705F, which is almost 96bytes to write, from the stm32cubeprogrammer manual -W64 command can to write, but is needs to be repeated 6 times, right?
Also from the manual there have write file for the OTP command "fwrite", how do i understand parameter "word" , can you tell me what command to use?
"STM32_Programmer_CLI.exe --connect port=usb1 -otp fwrite example.bin word=??"
example data:
47333934302D36313833304130314653323331353030303100FF71D2FFFFFFFF
66138B6F00FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF3106FFFFFFFF
41303100FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFD115FFFFFFFF
Can you tell me how it would be easier to write these data? thanks!
Solved! Go to Solution.
2024-05-20 7:52 AM
Hello @RJ3
Sorry for the late reply,
The "-otp" CLI is specific to the STM32MP series. For writing to OTP memory using CubeProgrammer on an STM32C031, you can simply use the following CLI:
>STM32_Programmer_CLI -c port=usb1 -d OTP_Data.bin 0x1FFF7000
Aziz
2024-04-21 7:58 PM
You could have a function or mode in your own software that writes the OTP settings you provide. You could presumably test if the are as expected or not.
2024-05-20 7:52 AM
Hello @RJ3
Sorry for the late reply,
The "-otp" CLI is specific to the STM32MP series. For writing to OTP memory using CubeProgrammer on an STM32C031, you can simply use the following CLI:
>STM32_Programmer_CLI -c port=usb1 -d OTP_Data.bin 0x1FFF7000
Aziz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.