2024-10-21 2:17 PM
I want to run STM32TrustedPackageCreator_CLI in docker. Unfortunately it requires a display, and is throwing an error without it:
qt.qpa.xcb: could not connect to display
qt.qpa.plugin: From 6.5.0, xcb-cursor0 or libxcb-cursor0 is needed to load the Qt xcb platform plugin.
qt.qpa.plugin: Could not load the Qt platform plugin "xcb" in "" even though it was found.
This application failed to start because no Qt platform plugin could be initialized. Reinstalling the application may fix this problem.
Available platform plugins are: vnc, minimalegl, linuxfb, wayland, wayland-egl, eglfs, xcb, vkkhrdisplay, offscreen, minimal.
Aborted (core dumped)
Is there a way to run it headless? CLI implies running without graphics?
2024-10-22 9:07 AM
Hello @imikec,
There is already a request to add Docker support for STM32TrustedPackageCreator_CLI.
Internal ticket number: 185103 (This is an internal tracking number and is not accessible or usable by customers).
If you need any further assistance with TPC_CLI, feel free to comment.
Amine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.