STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer 2.18.0 released

STM32CubeProgrammer v2.18.0 release information New features:  Added the support for the STM32N6 series– OTP programming– External memory programming– Serial boot via USB/UART– FSBL signature with stm32header V2.3 through the signing tool• Added the ...

Resolved! STM32F746G Discovery: Failed to erase memory

Originally a reply here: https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/stm32f746g-discovery-what-is-the-difference-between-cu2-and-cu4/m-p/746537/highlight/true#M40704  - moved to a new Thread for the new question. Thank you so much for you...

BA2 by Associate II
  • 2003 Views
  • 2 replies
  • 1 kudos

STM32CubeProgrammer 2.17.0 released

STM32CubeProgrammer v2.17.0 release information New features:• Added the support for the STM32MP25xx microprocessors in the STM32MP2 series – Flash memory and OTP programming, SSP support Added the support for devices in the STM32WB0 series: STM32WB0...

Resolved! STM32G071CBU6 DFU and UART Bricking issue

Just startet my small modbus therrmocouple project and im facing the issue with STM32G071CBU6.       First of all im not abble to connect via DFU usb, device isnt recognize i try reinstal stmCubeProgrammer, didnt change anything. Then try install dri...

stm32 dfu issue.png

Resolved! Bundled java Runtime missing or corrupted

I have installed new stm32programmer version 2.12.0 but when I try to lunch it i get this error in lunch4j plugin : This application was configured to use a bundled Java Runtime Environment, but the runtime is missing or corrupted. Any solution for t...

Ayouy.1 by Associate
  • 13235 Views
  • 4 replies
  • 1 kudos

STM32Cube Programmer CRC Error in post build

Hi,I'm using STM32H745ZI for Flash check using IAR tool checksum and STM32CubeProgrammer CLI it shows this error like this.................. D:\POST\bin\STM32_Programmer_CLI.exe -sl "D:\GitHub\gitdev\myCode/CM7/Exe/myCode.out" 0x08000000 0x08100000 0...

Lucifer37 by Associate III
  • 1360 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.