STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Can't program the option bytes using CLI?

Trying to program the option bytes I get the error message shown below. Can someone tell me what is wrong? I have tried with and without the displ and I have also tried with only one option byte at the time.C:\Temp\BMSM-18>"C:\Program Files\STMicroel...

thansen by Associate III
  • 281 Views
  • 4 replies
  • 2 kudos

Resolved! Error trying to install 32cubeprg 2.19.0 Linux

On Kubuntu 24.04 when double clicking onSetupSTM32CubeProgrammer-2.19.0.linuxan empty window appears and then closes again. If I runSetupSTM32CubeProgrammer-2.19.0.linuxvia the terminal (as admin or as user), I get this error:Exception in thread "AWT...

mx_ch by Associate II
  • 1505 Views
  • 5 replies
  • 1 kudos

STM32CubeProgrammer for macOS

It would be nice if the further versions could be running on case sensitive file system on macOS.Currently I need to use an USB key formatted APFS only. Then i can run the installer and install the programmer on this USB stick. As I most of the time ...

Laur59 by Associate
  • 239 Views
  • 1 replies
  • 0 kudos

Resolved! STM32_Programmer_CLI seg fault

I have an old Ubuntu 18.04 system which allows STM32CubeIDE to run, but the STM32_Programmer failed because libm.so and libc.so were wrong. I found glibc-2.30 and copied the libraries into the same directory as the STM32_Programmer lib. Now I just ge...

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32N6 flash failed to erase memory

I have a STM32N6570-DK and i can't seem to program it any more.  I tried it in both the STM32 programmer gui and terminal application.  So i can connect to the device read and read the flash but i can't seem to write to it any more.  I can't even era...

Screenshot from 2026-02-05 13-50-01.png Screenshot from 2026-02-05 13-50-37.png Screenshot from 2026-02-05 13-46-31.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.