2026-04-16 8:28 AM
It would be nice if the further versions could be running on case sensitive file system on macOS.
Currently I need to use an USB key formatted APFS only. Then i can run the installer and install the programmer on this USB stick. As I most of the time only need the command line tools (*CLI) I copied the binaries and some folders with data on my case sensitive disk. They work fine. Only the GUI is not possible on the case-sensitive file system.
2026-04-30 8:26 AM
Hello @Laur59 ,
I was able to recreate the same behavior, and I have forwarded your request to our development team to look further into it. (Internal ticket ID: 0062279)
I will let you know if there are any updates on this matter.
PS: Ticket ID: 0062279 is an internal tracking number and is not accessible or usable by customers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.