STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer 2.3.0 released

Dear communityWe are pleased to announce the release of STM32CubeProgrammer 2.3.0New features • Added the support of the STM32L4Pxxx and STM32L4Qxxx microcontrollers• Added the support of the STM32H7Axxx and STM32H7Bxxx microcontrollers • Added the b...

STM32CubeprogrammerAPI Qt build setting for Linux.

Hi fellas,System Info:Ubuntu 18.04 Virtual MachineQt Creator 5.12I am trying to implement example project of STM32CubeprogrammerAPI for qt on linux. However I am having problem at the compilation process. I use GCC as default compiler but STM32Cubepr...

bay.1 by Associate
  • 753 Views
  • 0 replies
  • 0 kudos

Flash Loader in Nucleo-STM32F401 (Unrecognized device)

Hi everyone.I have a board Nucleo-STM32F401, and i will try to write the program on STM32f401 with RS-232 communication, i did like in pdf, BOOT0 with jumper connect to Vcc (CN7 5pin+7pin) and i have the simple device RS232 to USB, and RX/TX connect ...

OMarc.1 by Associate III
  • 1430 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.