STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Program STM32 through bus CAN

Hello,Is it possible to program STM32* through bus CAN with STM32CubeProgrammer and STLINK-V3SET ?If yes :can we program only one STM32* even if many other STM32* are connected to the bus ?do we need to flash a bootloader or the embedded bootloader i...

ValentinG by Associate II
  • 1308 Views
  • 2 replies
  • 0 kudos

How to disable TZEN?

I try to unselect the TZEN flag to set it to 0 using STM32CubeProgrammer and it keeps reading back 1 after clicking apply.

Konami by Senior II
  • 1533 Views
  • 2 replies
  • 0 kudos

DFU not working on any STM32 board

NUCLEO boards are all not doing DFU: G031K8, L031K6, G431KB, G431RB, L452RE, L476RG, F401RE and of course the H743ZI the first version with STLINK2 None of those boards are seen by STMCUBE Programmer, in Windows 10 Device Manager USB section I never ...

KevinA by Senior
  • 1246 Views
  • 3 replies
  • 0 kudos

Option Bytes break Cube Programmer connection

I am trying to flash a STM32F303CCT6, and any time I try to set the Option Bytes to Level 1 protection it locks the board and breaks the connection. The only thing that is able to both see, and wipe the board is an android app.The board has WinUSB on...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.