2020-02-20 8:14 AM
commandline is:
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe -c port=COM9 br=115200 -q -log %logfile% -w %hexfile% -v -g 0x08000000
Is there a solution?
LOG for V2.3.0
16:07:44:325 Device name : STM32F405xx/F407xx/F415xx/F417xx
16:07:44:325 Sending Read command and its XOR:
16:07:44:325 byte 0x11 sent successfully to target
16:07:44:341 byte 0xEE sent successfully to target
16:07:44:341 Wait ends after 1 loop, dataready = 1, delay = 0
16:07:44:341 Received response from target: 0x79
16:07:44:341 Sending Read address and its checksum:
16:07:44:341 data sent successfully to target: 0x1ffff7ccdb
16:07:44:341 Wait ends after 1 loop, dataready = 1, delay = 0
16:07:44:341 Received response from target: 0x79
16:07:44:341 Sending number of bytes to be read - 1 and its checksum:
16:07:44:341 data sent successfully to target: 0x03fc
16:07:44:341 Received response from target: 0x1f
16:07:44:341
Response received from device: NACK
16:07:44:341
16:07:44:341 Error: Number of bytes to be be read at address: 0x1FFFF7CC not acknowledged!
16:07:44:341 failed to read the requested memory content
16:07:44:341 Could not read flash size at address 0x1ffff7cc
LOG for V2.2.0
14:50:52:908 Device name : STM32F405xx/F407xx/F415xx/F417xx
14:50:52:908 Device type : MCU
14:50:52:908 Device CPU : Cortex-M4
14:50:52:908
14:50:52:908 byte 0x11 sent successfully to target
14:50:52:908 byte 0xEE sent successfully to target
14:50:52:908 data sent successfully to target: 0x0800000008
14:50:52:908 byte 0x00 sent successfully to target
14:50:52:908 byte 0xFF sent successfully to target
14:50:52:924
14:50:52:924 Memory Programming ...
2020-02-20 11:16 PM
Hi @WBoei.1 ,
This will be internally checked.
Best Regards,
Khouloud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.