STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

DFU status response for STM32CubeProg

Hi,I've create my own bootloader with USB DFU functionality. (I need some function that built-in bootloader can't provide)I'm able to read/write/erase application firmware by USB DFU now.however, I find the STM32CubeProg work differently with built-i...

JWu.2 by Associate II
  • 2509 Views
  • 4 replies
  • 0 kudos

Resolved! programming a cortex-m0+ (STM32L073RB) device with a hex-file that uses not the whole memory or has leaks leads to wrong initial byte in flash memory of device

Hi everybody,I use the STM32CubeProgrammer version 2.3.0Following issue occurs during programming of a hex-file:1.) do a mass-erase or a clear of all sectors of the device2.) read out some bytes (for example the first sector)3.) the device-memory tab...

0693W000000WYiQQAW.png 0693W000000WYh8QAG.png 0693W000000WYhNQAW.png 0693W000000WYh3QAG.png
BNest.1 by Associate
  • 2462 Views
  • 4 replies
  • 1 kudos

How uncheck Option byte ?

I used STM32G070. According to the reference manual RM0454 rev2, it does not exist in this procesor Option byte IRHEN (in User Configuration). But the program allows you to set it.I did it, the processor stopped working, and no Option byte can now be...

Peko by Associate III
  • 3066 Views
  • 6 replies
  • 0 kudos

Different drivers DfuSe Demo vs. STM32CubeProgrammer

In order to see my microcontroller (G4 series) listed as Dfu device inside STM32CubeProgrammer the USB driver inside windows has to be of type "STM32 Bootloader"But to see it appear inside DfuSE Demo, the USB driver has to be of type "STM Device in D...

WSpar.1 by Associate III
  • 1475 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.