STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Hi. I have enabled PCROP protection in STM32CubeProgrammer and would like to disable it now. How do I disable it?

When I tried to do it in STM32CubeProgrammer I receive the next error:18:37:09 : OPTION BYTE PROGRAMMING VERIFICATION:18:37:09 : Error: Expected value for Option Byte "SPRMOD": 0x0, found: 0x118:37:09 : Error: Option Byte Programming failed

OKuro.1 by Associate II
  • 3489 Views
  • 3 replies
  • 0 kudos

Resolved! Error: No STM32 target found in STM32CubeProgrammer

Hi guys, I disabled flashing core M7 in STM32CubeProgrammer option bytes to run just M4, but now I cant connect to the board and the tool says Error: No STM32 target found!. Is there some possibility how to reset the option bytes to again run M7?Than...

binarybee by Associate III
  • 4355 Views
  • 8 replies
  • 0 kudos

Fail during download with bootloader in USB DFU mode

I have a custom board with a STM32H743ZI 144-pin processor. I can start the bootloader and the device is correctly recognized in the STM32CubeProgrammer as DFU in FS mode. I can read from device memory without issue, however when I try to download a ...

0693W000000WK1mQAG.png 0693W000000WK4lQAG.png
MLovr.1 by Associate II
  • 3697 Views
  • 5 replies
  • 0 kudos

Hot to update STM32F4DISCOVERY BOARD ST-LINK?

I did some AI examples at the STM32F4Disco Board. After that Cubeprog. doesn't connect to discoboard.When I connect the discoboard to my PC with usb, PC recognize the board but Cubeprog. doesn't connect to board.Error code is given below.12:45:29 : ...

Ogünd.1 by Associate
  • 1208 Views
  • 1 replies
  • 0 kudos

STM32H747 Dual Core Programming Both Cores

I have an application built in CubeIDE that utilizes both cores on the H747I-Disc1 board. The M4 core collects data and uses HSEM to notify the M7 core to process it. In debug mode I can run this just fine by first launching the M7, letting it run an...

RDock by Associate II
  • 5047 Views
  • 5 replies
  • 0 kudos

STM32CubeProgrammer - Bug report - External Loaders

Hello,Please move this to a more appropriate section if required, or let me know if there is a better way to report bugs.I have come across a couple of bugs whilst developing an STLDR for external flash access, note the memory arrangement of the flas...

0693W000000VN9wQAG.png
JHedges by Associate III
  • 3345 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.