STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Using Multiple ST-Links on the command line interface

I am building an application which will program 4 STM32G030 mounted on built PCBs in a test rig but cannot work out how to use 4 ST-Links connected to a USB hub in my test rig to do this. I need to run the ST-Links in parallel, not sequentially, to s...

AEmer.2 by Associate II
  • 4973 Views
  • 5 replies
  • 0 kudos

Stm32cubeprogrammer

Hi,​I just got a PCB with integrated stm32f0... Chip, which can be flash though ISP,usart, UART, Swd..​​But I downloaded the stm32cubeprogrammer to flash the chip as the hex and bin file was sent to me I keep getting the error o the bootloader stuff,...

AAkin.1 by Associate II
  • 5449 Views
  • 9 replies
  • 0 kudos

Resolved! [STM32H750] Can not upgrade the firmware by STM32CubeProgrammer when I have used the DTCMRAM section

[STM32H750]  Can not upgrade the firmware by STM32CubeProgrammer when I have used the DTCMRAM sectionjust add this code : the STM32CubeProgrammer will upgrade failed:​__attribute__((section(".DTCMRAM"))) uint8_t buf[2400] = {0};​int main(void){xxxx....

Davi by Associate II
  • 1474 Views
  • 1 replies
  • 0 kudos

Can't close app, if connection was failed.

Hello, i found next problem. If open app, and try connect to board with unsuccessful result, than app can't be closed any method, other than via task manager. In other case, app close via stantard button. This bug not disapering, if, for example, fir...

PGorb.1 by Associate
  • 4311 Views
  • 15 replies
  • 0 kudos

Resolved! How do I setup my Embitz to Debug with new L4Q5 MCUs ?

Hi everyone,I migrated to L4Q5 MCU and the Embitz debugger is not able to see the Target. I have pointed the build options to the new linker file. However, I feel like I need to translate STM32CubeProgrammer settings to the Embitz debugger options. W...

0693W000005AEn7QAG.png
VNado.1 by Associate III
  • 3221 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.