2020-02-01 3:26 AM
I'm trying to program STM32L031 microcontroller using STLINK but STM32CubeProgrammer gives me the following error:
Error: No STM32 target found!
These are the conditions:
1) The hardware is correctly connected because the STM32CubeIde emulates correctly the target
2) I have updated the STLINK firmware to the last firmware release
3) I have tested the programmer on another computer and I get the same error
4) I already tested to power cycle several times the target and the emulator but nothing changes
Can someone help me?
Thanks in advance
Paolo
2020-10-30 5:16 AM
Hi @PNenn.1
Please try with the last STM32CubeProgrammer then tell me if it solve the issue.
Best regards,
Nesrine
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.