STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Issue with STLink-server

Dear community supporters,I would like to add ability to share STM32 projects platforms to my team. I have setup a server on Debian 13 and setup the STLink server tool, and using a SSH tunnel to do port forwarding from the attached STLink port on the...

STM32 cli command on mac dont flash FW

Hello,I am experiencing a persistent verification error when flashing an STM32H7 via USB DFU using the STM32_Programmer_CLI. The exact same command and hardware work perfectly on Windows, but fail consistently on macOS.Environment:Tool: STM32CubeProg...

DanielAb by Associate
  • 330 Views
  • 0 replies
  • 0 kudos

Resolved! STlinkV3MODS_STM32 target not found.

Hi, I have brought 2 STlinkV3MODS. I have soldered wire at CN5 connector with 5+3 pin general connector to target the bluepill(not sure original or clone) the target MCU is STM32F103C8T6. when i select STlink at cube programmer shows error: debug aut...

BAS-BLEU by Associate III
  • 710 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.