STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

The difference between saving .bin and .elf files

I'm working with STM32H743 and W25Q128 external flash drive. I am trying to develop external loader. When I test with STM32CubeProgrammer and .bin files, everything works fine, writes to 0x90000000 address, verifies and reads OK. When I try to upload...

ISzum by Associate II
  • 8022 Views
  • 6 replies
  • 0 kudos

Error downloading Thread_SED_Coap_FreeRTOS

Hello thereI am using the official engineering code Thread_SED_Coap_FreeRTOS. When downloading with STM32CubeProgrammer, the error message connection to device0x495 is lost appears. At this time, the program should fail to download because the LED1, ...

0693W000006FJo9QAG.jpg 0693W000006FJqoQAG.jpg 0693W000006FJp2QAG.jpg
ZB.1 by Associate II
  • 2578 Views
  • 5 replies
  • 0 kudos

Resolved! cannot launch STM32CubeProgrammer

Hi,I just bought the STM32MP157F-EV1 and was trying to get it started.I tried to followed the manual written in the website and I thought I have completed step 4 and step 5 in the manual.However, when I tried to populate the SDCard, I realize that I ...

0693W000006Gpd6QAC.png 0693W000006GperQAC.png 0693W000006GpfLQAS.png
devinahw by Associate
  • 1412 Views
  • 1 replies
  • 0 kudos

Resolved! SWO viewer for STM32CubeProgrammer?

Hi,We're currently using the SWO viewer in the old ST-Link Utility in Windows.However, this is a bit inconvenient for us because our main development is in Linux. Is SWO support planned for STM32CubeProgrammer? Even just STM32Programmer_CLI SWO suppo...

Resolved! Boot loader with stm32CubeProgrammer

Thank you for helping.environment:MCU: STM32F769BIProgrammer: stm32CubeProgrammer Ver2.6.0I booted with the BOOT pin of the MCU set to H level and tried to write the hex file by the boot loader using USART1.It's progressing halfway, but I always get ...

Ebun.1 by Senior
  • 2758 Views
  • 5 replies
  • 0 kudos

Resolved! How to Data communicate with the STM32 BOOTLOADER ?

I want to make a Tool like STM32CubeProgrammer using MFC.When I checked the device monitoring, STM32CubeProgrammer was able to communicate 2K at a time.When connected via USB, the device manager shows up as STM32 BOOTLOADER, I am trying to connect th...

JPark.20 by Associate II
  • 1508 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.