STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! How to write FW to stm32g070 by CubeProgrammer via UART

I want to program the FW via UART.Read and erase function are working fine, but write function is not working with below error message.Anybody has a knowhow about this problem? 14:35:12 : Port configuration: parity = even, baudrate = 115200, data-bit...

EHeo.1 by Associate
  • 1251 Views
  • 1 replies
  • 0 kudos

STM32CubeProgrammer ZULU8 Jre recommended

STM32CubeProgrammer requires a Java™ Runtime Environment (JRE) to execute and In April 2019, Oracle decided to change their economic model around Java.Since this date the Oracle JVM beyond version 1.8u211 becomes non-free for professional usageFor S...

Unable to run stm32cubeprogrammer due to Java issue

I get the following error when I try to run STM32CubeProgrammer both as admin or non-admin. My system details: Windows 10Java versions : I have tried using cubeprogrammer 2.5 as well as 2.4 and I get the same error in both cases. Please let me know i...

GRang.1 by Associate II
  • 6288 Views
  • 4 replies
  • 0 kudos

Hi, I reacently desgined my first custom STM32 hardware. I am using an STM32L432KCUx controller and the firmware i programmed it with does not seem to be executed.

I use Cube Programmer V2.4 and i am programming the chip using USB DFU mode. Its a simple firmware with a blinking LED to get to know how programming unsing DFU works. I tested the firmware on the NUCLEO L432kc board and there it seems to work fine.T...

DKers.1 by Associate II
  • 2672 Views
  • 7 replies
  • 0 kudos

Resolved! No OptionByte setting from file

I am trying to migrate from UM0462 Flash Loader Demonstrator to the STM32CubeProgrammer (upon a recommendation from STM, as the former becomes obsolete). Yet I seem to be missing the option of loading OptionByte file.The documentation for cube refers...

0693W000005CCnsQAG.jpg
DarkLight by Associate II
  • 2371 Views
  • 4 replies
  • 0 kudos

STM32FG031 once pin 4 (PF0 - NRST) is set as GPIO input, it is not possible to reprogram the MCU flash. How to recover ?

Working with a STM32G0316-DISCO, I was so stupid I wrote a test program where I set pin 4 (NRST) as GPIO input (PA0). It goes without saying that now I'm not able to reprogram che MCU. Is there any magic trick to get out of this situation aside buyin...

Frabs by Associate II
  • 2743 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.