STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer 2.9.0 released

New features• Updated the programming mechanism for the STM32U575/585 microcontrollers via a flash loader usage in TZEN = 0, and a new programming mode in TZEN = 1 (fast/reliable)• Added double authentication and user keys provisioning via JTAG for t...

Resolved! Can't use STM32CubeProgrammer API

Hi everyone,I'm trying to develop my own console project in C++ on Visual Studio using the SMT32 API to download and verify an STM32 CPU and I need your help please.I can build my solution with no error but I can't run it. I get : The Application was...

ABeyb.1 by Associate
  • 2636 Views
  • 4 replies
  • 0 kudos

Cannot Run after programming in CubeProgrammer via UART

I have a question about the flash program function by UART communication on the evaluation board NUCLEO-L433RC-P.After rewriting flash with UART, I restarted it with Run After Program, but it does not work properly (LED blinks if it is normal).Unplug...

0693W00000HppUCQAZ.png 0693W00000HppU7QAJ.png
Yoshi1 by Associate III
  • 7234 Views
  • 12 replies
  • 0 kudos

Resolved! Missing Database files

Hi everyone,I'm working on STM32f407VG discovery board on linux 20.04 host machine. I've written my own bootloader code starting at address 0x08000000. But when I'm trying to upload my firmware using STM32Cube Programmer its giving me error saying, d...

0693W00000HpqYtQAJ.png
Rsrma.1 by Associate III
  • 5628 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.