STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! stm32F103R8 chip programming problem

HiIt's just that something strange happened to meIf I use RKit-ARM 1.68.18.0108 I get the following CheckSum "D9D0460"But if I upgrade RKit-ARM to 1.72.19.0253, there will be a version error problemBut 1.72.19.0253 is to fix the problem of CheckSum d...

0693W00000JMSwIQAX.jpg 0693W00000JMSwbQAH.jpg
TOPGUN by Associate II
  • 2457 Views
  • 5 replies
  • 0 kudos

Resolved! GETID command not acknowledged

Hi everyone, I'm writing my own bootloader for STM32f407VG, in the start address of flash memory. But getting problem GetID command is not acknowledged. I've attached a log also. 10:49:19:443 : RTS low 10:49:19:443 : DTR low 10:49:19:443 : Serial...

Rsrma.1 by Associate III
  • 5885 Views
  • 5 replies
  • 0 kudos

STM32H7A3ZIT6 Half Flash Bricked/Corrupted

Hi,I'm facing this weird behavior with many STM32H7A3ZIT6 parts, where after we flash our Firmware, the MCU do not work and when we read the flash content, we can notice that one flash bank (1MB) is either corrupted with random data or erased. Someti...

0693W00000JMZvCQAX.png 0693W00000JMZvqQAH.png 0693W00000JMZu1QAH.png 0693W00000JMZyBQAX.jpg
DReis.2 by Associate II
  • 1628 Views
  • 2 replies
  • 0 kudos

Trouble installing STM32CubeProgrammer

Hi,I am trying to install SetupSTM32CubeProgrammer_win64 and I am seeing some issues I don't understand.This is the path selected by default.when I enter Next I get this errorSo I created a separate directory and moved forward while installing this e...

0693W00000JMb11QAD.png 0693W00000JMb1aQAD.png 0693W00000JMb29QAD.png 0693W00000JMb2OQAT.png
MK8290 by Associate II
  • 1451 Views
  • 2 replies
  • 0 kudos

Resolved! connect error ST-LINK on 'STM32H7XI-DISCO'

I can't connect the STM32H7XI-disco board with the PC.At first, it was connected through ST-Link.I connected to the PC using a micro Btype cable to ST-LINK V3E (CN2) on the board.However, it is not connected after the wrong version of download.I want...

STM32_Programmer_CLI.exe bug?

Hey all,I use the STM32CubeProgrammer v2.8.0.I want to display the ITM messages on the console with the following command. STM32_Programmer_CLI.exe -c port=swd sn=0677FF555054877567083453 -swv freq=216 portnumber=23The problem is that the parameter "...

bionix by Associate
  • 1172 Views
  • 2 replies
  • 0 kudos

How to use STM32CubeProgrammer on a Mac?

I want to download a DFU file to a target using STM32CubeProgrammer (2.9.0) running on the MacOS. I can connect to the target and read its memory contents OK, but when I try to open a DFU file, the filename is grayed-out. The manual does not mentio...

EHans.1 by Associate
  • 2067 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.