2025-09-12 7:47 AM
I recently tried to use -noreconnect via the cli on windows and it still attempted to reconnect.
I was connected via UART and programming option bytes.
Here was the command I used:
& "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -c port=COM14 br=115200 -noreconnect -ob ndbank=0x0
I see that there was fix put in for linux. Im wondering if the same bug exists on Windows.
Thanks,
Daniel
Solved! Go to Solution.
2025-09-22 12:52 AM
Hello All,
Thank you for posting and for all the details you provided.
I escalated this issue to the relevant team (through internal ticket number 218005) to take a closer look at the problem.
(PS: ticket number 218005 is an internal tracking number and is not accessible or usable by customers).
2025-09-15 3:47 PM
2025-09-17 4:16 AM
I'm having the same issue when using API v2.20 on Windows.
2025-09-17 6:59 AM
Thanks for the confirmation and work arounds.
I assumed posting here was filing the bug with ST. Is there a different place for that?
Daniel
2025-09-22 12:52 AM
Hello All,
Thank you for posting and for all the details you provided.
I escalated this issue to the relevant team (through internal ticket number 218005) to take a closer look at the problem.
(PS: ticket number 218005 is an internal tracking number and is not accessible or usable by customers).
2025-10-08 2:14 PM
Hi All,
We confirm this issue.
Thank you again for highlighting this issue. Your feedback has been very helpful in raising the ticket along to our development team for fix.
2026-02-10 12:44 AM
I'm using STM32CubeProgrammer API but I don't find the command to no reconnect to device after OB programming. Could you list the procedure to do that? Thanks
2026-02-12 12:53 PM
Just like to echo this thread and add that the -noreconnect command still doesn't seem work for STM32CubeProgrammer v2.21.0 on Windows 11
Looking forward to a fixed release.
Thanks,
Eric
2026-02-25 2:22 AM
Hello all,
Issue is fixed in the latest STM32CubeProgrammer release available here.
Aziz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.