2019-12-23 4:05 PM
Hi, i am using stm32f4. in my project i have one transmitter and one receiver.
i transmit an 2 byte integer value using
HAL_UART_Transmit(&huart1,&temp_byte1,sizeof(temp_byte1), 500);
HAL_UART_Transmit(&huart1,&temp_byte2,sizeof(temp_byte2), 500);and on the receiver part. i read these values using
void USART6_IRQHandler(void)
{
HAL_UART_Receive_IT(&huart6,&rx_data,1);
temp_data[rx_index]=rx_data;
rx_index++;
if(rx_index==2)
{
rx_index=0;
temp = ((temp_data[0]<<8)|temp_data[1]);
if(temp!=79){ //sometimes i see a 79 in my buffer!
hc05_flag = 3; //irrelevant flag with this question
nm=0; //irrelevant flag with this question
}
}it works fine for one time. but after, i see temp_data[1] in temp_data[0]. it shift 8 bits and i see a big temp value (63744 etc.) . where is my problem?
2019-12-23 5:40 PM
My guess is that this is a classroom exercise.
Your problem is that you have two processes and no method to synchronize related transmits and receives.
Its your project. I will leave it up to you to figure out how to keep them in sync.
Cheers, Hal
2019-12-23 6:34 PM
HAL_UART_Receive_IT() does not work like this. You need to collect the data in the callback, as the function you're using should return immediately, not when it actually has data.
2019-12-23 11:20 PM
You must use HAL_UART_IRQHandler() and HAL_UART_RxCpltCallback().
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.