2019-12-16 9:50 AM
2019-12-16 1:09 PM
This appears to be a Cube-specific symbol, defined in [CubeF3]\Drivers\STM32F3xx_HAL_Driver\Inc\stm32f3xx_hal_adc_ex.h , Do you have this header included in your source files?
JW
2019-12-18 11:01 PM
I apologize, I meant "ADC_EXTERNALTRIGCONV_T2_CC2" is not defined. In stm32f3xx_hal_adc_ex.h, it is defined
#if defined(STM32F301x8) || defined(STM32F302x8) || defined(STM32F318xx)
/* List of external triggers with generic trigger name, sorted by trigger */
/* name: */
/* External triggers of regular group for ADC1 */
#define ADC_EXTERNALTRIGCONV_T1_CC1 ADC1_EXTERNALTRIG_T1_CC1
#define ADC_EXTERNALTRIGCONV_T1_CC2 ADC1_EXTERNALTRIG_T1_CC2
#define ADC_EXTERNALTRIGCONV_T1_CC3 ADC1_EXTERNALTRIG_T1_CC3
#define ADC_EXTERNALTRIGCONV_EXT_IT11 ADC1_EXTERNALTRIG_EXT_IT11
#define ADC_EXTERNALTRIGCONV_T1_TRGO ADC1_EXTERNALTRIG_T1_TRGO
#define ADC_EXTERNALTRIGCONV_T1_TRGO2 ADC1_EXTERNALTRIG_T1_TRGO2
#define ADC_EXTERNALTRIGCONV_T2_TRGO ADC1_EXTERNALTRIG_T2_TRGO
#define ADC_EXTERNALTRIGCONV_T6_TRGO ADC1_EXTERNALTRIG_T6_TRGO
#define ADC_EXTERNALTRIGCONV_T15_TRGO ADC1_EXTERNALTRIG_T15_TRGO
#define ADC_SOFTWARE_START (0x00000001U)
#endif /* STM32F301x8 || STM32F302x8 || STM32F318xx */But in CubeMX, you can select ADC_EXTERNALTRIGCONV_T2_CC2 which leads to an "undefined" error.
2019-12-19 12:17 AM
OK so this appears to be a CubeMX-specific problem, correct?
@Khouloud ZEMMELI can you please have a look at this? Thanks.
JW
2019-12-19 12:56 AM
Hello @Patrick Chwalek , Could you please share your ioc file ? need to know the MX version.
Best Regards,
Khouloud
2019-12-19 1:09 AM
Thanks Patrick for the feedback, this will be internally checked.
Best Regards,
Khouloud.
2019-12-23 4:06 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.