2021-03-19 3:38 AM
osram_init(3,1,2,6); // Initialized with Prescaler=3, HighSelect=1, tRWR=2,tACC=6, MemoryMap, refer to CUBE-MX L4R9Eval OSPI_MemoryMap example Project
uint8_t* mem_addr = ( uint8_t * )( OCTOSPI1_BASE + 0 );
*mem_addr = 0xF0;
*(mem_addr+1) = 0xF1;
*(mem_addr+2) = 0xF2;
*(mem_addr+2) = *(mem_addr+1); // 0x90000002=0xF1? Work
*(mem_addr+3) = *(mem_addr+1); // 0x90000003=0xF1? does'nt work
*(mem_addr+4) = *(mem_addr+1); // 0x90000004=0xF1? work
// desc order
*(mem_addr+2) = 0xF2; // ok
*(mem_addr+3) = 0xF3; // error, set to 0x90000002
*(mem_addr+4) = 0xF4; // ok
*(mem_addr+1) = *(mem_addr+2); // 0x90000001=0xF2? error. value set to 0x90000000
*(mem_addr+1) = *(mem_addr+3); // 0x90000001=0xF3? error. value set to 0x90000000
*(mem_addr+1) = *(mem_addr+4); // 0x90000001=0xF4? error. value set to 0x90000000
can't assign value by access it's self.
can someone help me?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.