STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! SMBus STM32F439 HAL Driver

Hi all,I read STM32F4 MCU family doesn't support SMBus because of hardware limitations in the I2C cell. For this reason SMBus is not included in the HAL driver. If I choose STM32F439ZI in STM32CubeMX and I activate I2C, I can select between 3 differe...

0693W000008x25NQAQ.jpg
AFara.2 by Associate II
  • 2946 Views
  • 2 replies
  • 0 kudos

Bug in UART code generation in STM32CubeIDE 1.4.2 ?

I upgraded from STM32CubeIDE 1.3.1 to 1.4.2, and got issues with UART speed. To eliminate error sources, I just made a minimum project with UART transmit. At 115200bps, the bit-time should be 8.68us (and it is with IDE1.3.1), but it comes out as 7.82...

DVeda.1 by Associate II
  • 4148 Views
  • 9 replies
  • 0 kudos

SDIO FATFS with cube IDE

Hi,I tried to use SDIO with 4 bit and 1 bit mode with FatFS. I use STM32F407 Discovery board and I wired a micro SD card board to it. The SD card is a 16 GB micro SDHC card formatted to FAT32. I used STM32cubemx V6.2 .0 and Atollic TrueSTUDIO for S...

MHass.2 by Associate III
  • 1440 Views
  • 1 replies
  • 1 kudos

Resolved! Test the UIF Flag

I am newbie getting lost in the HAL functions/features to use. I use STM32CubeMx to generate the code and use Keil uvision5 for development. I use STM32G071 Nucleo-64 development kit.  I wish to measure a ‘start’ pulse of a proprietary protocol. The ...

HThak.2 by Associate
  • 2335 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.