2025-01-15 7:02 AM
MCU:STM32U585xx
Env:ThreadX + USBX + FileX
I want to use USBX add my own class type, but I'm already have 3 classes, HID, MSC and CDC ACM, it means 4 classes after added my own.
In file (ux_device_descriptors.h) have a define (USBD_MAX_SUPPORTED_CLASS 3U), this value determined the (tclasslist) array size, also the framework max class, can not be changed by user define or STM32CubeMX(no option find).
If I change this define, it will be overwrite by STM32CubeMX when generated code. How can I do this correctly?
Solved! Go to Solution.
2025-04-07 2:07 AM
Hi @Jason927
Using latest CubeMX version, it is supported on H5 not sure on U5. So, ensure that there is enough RAM, stack and heap memory allocated, configuration descriptor to handle the additional class in USBX.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-07 2:07 AM
Hi @Jason927
Using latest CubeMX version, it is supported on H5 not sure on U5. So, ensure that there is enough RAM, stack and heap memory allocated, configuration descriptor to handle the additional class in USBX.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.