2022-12-29 8:53 AM
I created a new project from a downloaded example Nx_TCP_Echo_Server for a Nucleo board. But when I attempt to edit the CubeMX .ioc file, I get the error listed above. I can't find a way to edit the .ioc file or upgrade CubeMX to V6.6. Can anyone offer suggestions?
2022-12-29 9:19 AM
A suggestion: try a bit harder to install latest CubeMX (6.7.0 or at least 6.6.1). Here.
Upgrade is not quite reliable. Download the installer and do a full install.
It can be installed side by side with your current version (6.2.1) if you still need the latter.
2022-12-29 9:39 AM
Pavel,
Thanks for the help. I should have stated that the CubeMX that I am attempting to use is the integrated version inside of the recently installed CubeIDE(Version: 1.6.1). I have tried updating CubeIDE, but the updater states that my current version has no updates.
So I did download and install CubeMX V6.7 separately from CubeIDE, and it DOES open the .ioc file inside of my project.
So the "integrated" CubeMX is of no use unless I can find a way to update it......seems a little counter-intuitive. Is there a way to update the integrated CubeMX?
2022-12-29 11:22 AM
The current CubeIDE version is 1.11. Why did you install an outdated version?
2022-12-30 1:43 PM
gbm...thanks for pointing that out. Looks like I updated 1.6 instead of installing 1.11. All working now.
2022-12-30 8:07 PM
> So the "integrated" CubeMX is of no use unless I can find a way to update it......seems a little counter-intuitive.
Yes, this is what I learned after several years with CubeMX and IDE. Using a standalone CubeMX allows updating it independently from CubeIDE. You can install several versions of it.
I don't use the integrated Cube of CubeIDE.
CubeIDE itself (Eclipse, debugger) is more stable and I don't feel pressure to update it since v 1.7.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.