2023-01-02 11:24 AM
I try to implement an FFT on the STM32F429I controller. I succeeded in accessing cmsis files and compilation worked fine by including arm_math.h and libarm_cortexM4lf_math.a. in CubeIDE Version: 1.8.
However, when I try to debug the program, it goes into the HardFault_Handler().
If I execute the program in singel stepping (pressing F5), I get the following information:
Can't find a source file at "C:\CMSIS\CMSIS_Setup_V4.xx\CMSIS\DSP_Lib\Source\GCC/../TransformFunctions/arm_rfft_q15.c"
2023-01-02 12:34 PM
the ***.a lib is compiled, not source.
so you cannot see the source, because there is no source code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.