2019-06-13 6:18 AM
Code generated using LL : (Issue)
------------------------------------------
void SystemClock_Config(void)
{
LL_FLASH_SetLatency(LL_FLASH_LATENCY_0);
if(LL_FLASH_GetLatency() != LL_FLASH_LATENCY_0)
{
Error_Handler();
}
LL_RCC_HSI_Enable();
/* Wait till HSI is ready */
while(LL_RCC_HSI_IsReady() != 1)
{
}
LL_RCC_HSI_SetCalibTrimming(16);
LL_RCC_HSI48_Enable();
/* Wait till HSI48 is ready */
while(LL_RCC_HSI48_IsReady() != 1)
{
}
LL_RCC_PLL_ConfigDomain_SYS(LL_RCC_PLLSOURCE_HSI, LL_RCC_PLL_MUL_6, LL_RCC_PREDIV_DIV_1);
LL_RCC_PLL_Enable();
/* Wait till PLL is ready */
while(LL_RCC_PLL_IsReady() != 1)
{
}
LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_2);
LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_1);
LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL);
/* Wait till System clock is ready */
while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_PLL)
{
}
LL_Init1msTick(24000000);
LL_SYSTICK_SetClkSource(LL_SYSTICK_CLKSOURCE_HCLK);
LL_SetSystemCoreClock(24000000);
LL_RCC_SetUSARTClockSource(LL_RCC_USART2_CLKSOURCE_SYSCLK);
LL_RCC_SetUSBClockSource(LL_RCC_USB_CLKSOURCE_HSI48);
}
Code generated using HAL (Working Fine)
--------------------------------------
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/**Initializes the CPU, AHB and APB busses clocks
*/
//__HAL_RCC_PWR_CLK_ENABLE();
//__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
//__HAL_RCC_PWR_CLK_DISABLE();
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI48;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USB|RCC_PERIPHCLK_USART2;
PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_SYSCLK;
PeriphClkInit.UsbClockSelection = RCC_USBCLKSOURCE_HSI48;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure the Systick interrupt time
*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick
*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
#endif
2020-12-02 2:51 AM
This could be the same issue as described in
https://community.st.com/s/question/0D50X0000B41tlASQQ/stm32h743-hsi-frequency-waaaayyy-off
So in
LL_RCC_HSI_SetCalibTrimming(16);16 is wrong and should be 64 (or maybe different for STM32F072xb).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.