2021-09-03 9:32 AM
Hello,
I'm trying to use a timer to measure the frequency of an input signal using the callback function:
HAL_TIM_IC_CaptureCallBack(TIM_HandleTypeDef*htim)
The function never seems to be called when a voltage is applied to the input pin.
Here is the timer initialization code, TIM1 interrupts have been enabled. Any suggestions as to why the callback function is not working will be appreciated.
static void MX_TIM1_Init(void)
{
/* USER CODE BEGIN TIM1_Init 0 */
/* USER CODE END TIM1_Init 0 */
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_IC_InitTypeDef sConfigIC = {0};
/* USER CODE BEGIN TIM1_Init 1 */
/* USER CODE END TIM1_Init 1 */
htim1.Instance = TIM1;
htim1.Init.Prescaler = 8000-1;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 65535;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_IC_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;
sConfigIC.ICFilter = 0;
if (HAL_TIM_IC_ConfigChannel(&htim1, &sConfigIC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM1_Init 2 */
/* USER CODE END TIM1_Init 2 */
}
2021-09-03 10:02 AM
Have you called the following?
HAL_TIM_IC_Start_IT(&htim1, TIM_CHANNEL_1)Did you generate this code with CubeMx?
2021-09-03 11:12 AM
2021-09-03 11:55 AM
Try getting an example to work:
> The function never seems to be called when a voltage is applied to the input pin.
Note that the pin needs to be low first, then transition high in order for the callback to work. If it's already high, nothing happens.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.