2018-05-19 1:48 AM
Hi,
I can not get the input compare mode working as expected. I need to use TIM2 CH1 as trigger to measure the frequency of external pulses. I have used the methode on a STM32F091 where it works fine.
RCC and GPIO are initialized. And I will get a CC1IF interrupt as soon as I connect the external signal source BUT CCR1 is always 0! It seems to me the counter is not counting. My code to set up the counter:
#define VEL_CLK 10000000 //System is running at 200 MHz PSC is set to 4
TIM2->CCMR1 = TIM_CCMR1_CC1S_0 ; // ch 1 for input capture
TIM2->SMCR = TIM_SMCR_ETP | TIM_SMCR_SMS_2 | TIM_SMCR_TS_2; // reset mode on ch1TIM2->CCER = TIM_CCER_CC1P | TIM_CCER_CC1E;
TIM2->PSC = (APB1_CLK / (VEL_CLK)) - 1; // Timer clock
TIM2->CR1 = TIM_CR1_CEN; // Start timer TIM2->DIER = TIM_DIER_CC1IE; NVIC_SetPriority(TIM2_IRQn,0); NVIC_EnableIRQ(TIM2_IRQn);The TIM2 registers after intialization (see attached file).
Any suggestions very appreciated!
Best regards
Dirk
2018-05-29 1:34 AM
That is right Jan, normally I am never using the CubeMX generated code, but for this project I tried it for the first time to get the board running faster and in order to get the USB stack supplied by ST running. As soon as time permits I will clean out all HAL calls where it is possible.
About ARR the RM says so all my fault:
In upcounting mode, the counter counts from 0 to the auto-reload value (content of the
TIMx_ARR register), then restarts from 0 and generates a counter overflow event.Dirk
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.