2025-06-17 11:58 PM
Hi,
when looking into the schematics of the STM32H735G-DK board (MB1520B), the Ethernet-PHY is connected via RMII.
Now when I configure RMII for an STM32H7 in CubeMX, the interface pins do fit properly to what is used in the MB1520B schematics - except the RX_ERR-line. According to the schematics it is connected to PB10, but when I enable PB10 in CubeMX for use as RX_ERR, it is marked in yellow with the remark "no mode".
So...how do fit both things together? How can I enable RX_ERR being used in Cube MX for RMII-mode?
Thanks!
Solved! Go to Solution.
2025-06-24 4:14 AM
Not an error! You could still set the GPIO to interrupt mode, or poll it.
Anyway, Cube is not perfect...
Edit: found it in the datasheet!
But the H7 ETH-peripheral's RMII doesn't do anything with that pin, except that it sets a bit in an RX descriptor.
Still not sure if that's the case for MII or RMII, in the datasheet it's called only " MII_RX_ER ", all RMII signals are usually called " RMII_* ".
Is the signal connected to the PHY ?
2025-06-18 1:00 AM - edited 2025-06-18 1:01 AM
Check the datasheet for the alternate functions, I faintly remember that RX_ERR is simply not supported by the H7 hardware. But I might be wrong.
And it's definitely RMII, without the "G". ;)
2025-06-23 11:48 PM
So this would be an error in the evaluation board from ST then!?
2025-06-24 4:14 AM
Not an error! You could still set the GPIO to interrupt mode, or poll it.
Anyway, Cube is not perfect...
Edit: found it in the datasheet!
But the H7 ETH-peripheral's RMII doesn't do anything with that pin, except that it sets a bit in an RX descriptor.
Still not sure if that's the case for MII or RMII, in the datasheet it's called only " MII_RX_ER ", all RMII signals are usually called " RMII_* ".
Is the signal connected to the PHY ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.