2014-03-04 10:42 AM
Hi
I'm exploring the STM32F405 and for this, i wanted to create the initial project with the Cube MX tool.
I've settet all the things up to my configuration. In minimal i just set the hole clock thing up.
I've burned this down to the chip just to make sure if the thing going to my while(1).
But the generated code leads to the Hardfault error handler.
I discovered that the fault is happening somewhere around when it calculates the latency for flash read write.
This is in the beginning of the method: HAL_RCC_ClockConfig located in stm32f4xx_hal_rcc.c
It jumps directly after command '' if(RCC_ClkInitStruct->SYSCLKSource == RCC_SYSCLKSOURCE_HSE) '' (Line 782) to Address 0
I don't think that i have to change some lines in the library..
Probably the clock is set the wrong way.
here are the values out of the generated code:
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.LSEState = RCC_LSE_BYPASS;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 6;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 10;
RCC_OscInitStruct.PLL.PLLN = 210;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 7;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0);
#cubemx #stm32f42014-03-04 10:51 AM
Your problem is similar to this one:
A solution has been posted (redefine theFLASH_LATENCY_0
constant to the correct value). This bug has been already fixed in our development tree currently under validation Regards Daniel2014-03-04 10:55 AM
Realistically if you're running the processor at 168 MHz, the flash latency is going to need to be 5
The Hard Fault handler should be able to point you at exactly what assembler instruction caused the fault, you should then inspect that code and the internal registers to determine the cause.2014-03-05 12:08 PM
Hi,
Hanks for the fast Answers,
As i know i have 2 different errors. One is that related to the wrong latency which jumped to address zero. Then the other which leads to the harderror.
But also the harderror fault does not have to be happen with just the initial generated code base. I have no activated interrupts (just systick).
Up to now i didnt had the time to explore more.But thanks for pointing out the latency error.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.