2015-10-06 11:19 PM
have you ever noticed, that pinout and clock config tabs aren't matching each other?
especially if you select Nucleo or Discovery Boards, on pinout Tab you can see pin's selected and marked properly, but Clock configuration tab doesn't reflect proper crystals ...for STM32F4 Discovery there is an issue with clocking ratios so when you move to clock config tab mostly it is red overclocked... for STM32F466RET Nucleo board, it doesn't reflect 32 kHz crystal connected to the MCU PC14,PC15... #stm32 #cubemx2015-10-07 8:02 AM
Hi nadiradze.nikoloz,
Which version of CubeMx are you using? -Shahrzad-2015-10-09 4:50 PM
Yes, I did notice that in an old version of the tool. Download the current versions of CubeMX and the F4 modules and the clock tree is correct.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.