STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32CubeMX Issues

Posted on October 07, 2015 at 08:19have you ever noticed, that pinout and clock config tabs aren't matching each other?especially if you select Nucleo or Discovery Boards, on pinout Tab you can see pin's selected and marked properly, but Clock confi...

nadiradn by Associate
  • 995 Views
  • 2 replies
  • 0 kudos

STM32Cube I2C HAL Issues with HTU21D and BMP180

Posted on October 07, 2015 at 13:16 I am a beginner to STM So far, I have done a lot of work on NETMF and AVR. Starting out with STM Environment: I have a super tiny board for STM32F103C8 (like this one http://artofcircuits.com/pro...

CubeMX Newbie Question

Posted on October 03, 2015 at 05:00I intend to use SDIO with STM32F103C8 MCU and am trying to generate initialization code from CubeMX.It turns out, SDIO is NOT available for STM32F103C8 MCU in CubeMX.  Is there a good reason why this cannot be done...

ymhsieh by Associate II
  • 1472 Views
  • 4 replies
  • 0 kudos

Possible bug in STCubeMX HAL DMA code for F4

Posted on August 13, 2014 at 02:14I do not know enough about the internal workings of the processor to be sure, but I believe there is a bug in the HAL DMA drivers for the F4xx series. Specifically, it seems the De-init method puts the DMA periphera...

jwoolston by Associate II
  • 1645 Views
  • 3 replies
  • 0 kudos

Stm32Cube - Simulink - MikroC

Posted on October 01, 2015 at 13:22Hello, I'm new here and i've the problem that i don't know how to get the generated code from simulink and CubeMX to my Microcontroller.My Setup:I use mikroC Pro and an EasyMX Prov7 board with STM32V107VCT6Now I go...

Problem with USB Host CDC class

Posted on July 03, 2014 at 12:01Hello,I'm using STM32CubeMX to generate a project for STM32F207 that uses USB Host. The project compiles without problems. I have a custom USB device that uses CDC to send and receive serial data. When the device is a...

BUG: CAN race condition if HAL_CAN_Receive_IT is used

Posted on April 15, 2015 at 22:27 If you use HAL_CAN_Receive_IT for receive and send messages at same time you can get race condition. Typical callback looks like: void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef* CanHandle) { if ((CanHandle...

vromanov by Associate II
  • 4051 Views
  • 6 replies
  • 0 kudos

Request STM32cubeMX to work with latest Java

Posted on July 23, 2015 at 09:41Due to security reasons I recently updated to the latest Java 8 Update 51 (Releasedate 14.07.2015) and deleted the old Java version. But now CubeMX (4.9.0) is not starting anymore asking for an old Java 1.7.0_45 I kin...

ramm by Associate II
  • 1404 Views
  • 5 replies
  • 0 kudos

STM32F103 HAL UART: TX error, HAL_BUSY (FreeRTOS)

Posted on September 12, 2015 at 00:46Hi All,I'm trying to build an application which can receive commands through UART, and can also send messages.I have created 2 threads using FreeRTOS: one for a continuous RX, and one for a repetitive TX.The RX t...

balazs by Associate II
  • 1337 Views
  • 1 replies
  • 0 kudos

need very simple UART RXNE and IDLE interrupt example

Posted on September 08, 2015 at 12:25 Hello, I've used the STD peripheral libraries before and successfully generating interrupts from UART //snippet 1 void USART1_IRQHandler(void){ char chee; if(USART_GetITStatus(USART1, U...

krishna2 by Associate
  • 7763 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.