2020-05-11 6:49 PM
2020-05-11 8:08 PM
Not sure I can unpack that.
If the hardware as described in the Reference Manual seems capable of the task, code and test the concepts by programming the hardware directly, and not via the abstraction/obfuscation layer.
2020-05-12 10:43 AM
Yes, that's the ultimate step to get things to work in the absence of tools support..but it requires long..many days if not weeks long..efforts..
2020-05-12 10:59 AM
The application seems niche, and complex, the teams with solutions are probably working on closed source projects. ie needs a properly architected solution, or needs to fit an existing infrastructure, and is not amenable to a causal one-size-fits-all demo.
Suggest you engage with your FAE to see if any help/resources are available, or if they can recommend contractors with specific competence.
2020-05-12 12:12 PM
Appreciate your quick and always valuable answers and feedback.
Descriptor based cyclic multibuffer use is quite a common scenario in high speed data captures be it audio, video etc. I use it all the time in many DSP and FPGA architectures (with ARM SoC etc). It frees the cpu from reprogramming the DMA after each cycle to avoid over writing the buffers by switching to another buffer automatically at the end of a cycle.
In many architectures it is implemented as Scatter-Gather DMA with several flexible features to perform these complex and varied data capture operations with no cpu interventions at all, all via pre-programed DMA descriptors.
But in STM32 DMAs, there's no descriptor feature supported and this alternate multibuffer scheme (actually it's only a double-buffer) helps somewhat by enabling the use of a ping-pong buffer scheme which is ok for such uses with proper programming design.
I use the DFSDM block which is a very useful block for advanced audio captures from PDM microphones with custom sampling rates, resolutions, multiplexing etc possible compared to other schemes. But all these are useful only if such a multibuffer DMA is used. In the sample applications provided by ST Micro, a simple very inefficient dma scheme is used where one needs to use cpu to copy half the buffers by enabling the Half-Buffer Complete DMA interrupts. It's ok for simple, low-speed applications but not for high-speed, complex applications. (in fact in my use it miserabley fails when I increase the data rates.
Anyway, I'll have figure out using the best way to implement this scheme by directly controlling the DFSDM block and the DMA controller etc.
Again, thanks for your inputs..best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.