2025-06-11 9:33 AM - edited 2025-06-11 9:40 AM
I am having a hard time to set up a STM32 project in VS Code that works with all C++ features.
I set up my CMakeLists and enabled CXX language and add all my sources and so on.
When I keep my main.c and get my c++ functions with extern form a cpp file, the compiler does not find c++ functions like <cmath> that I include in my hpp headers.
I also tried setting up a project that I could open in VS Code and CubeIDE. In Cube IDE I renamed the main.c to main.cpp . And there in Cube IDE everything compiles fine.
In VS Code I get errors for the same project like and <cmath> is only found when I manually include the arm-none-eabi folder:
undefined reference to `MX_SPI1_Init'",
What is the best way transform a CMake project from CubeMX to C++?
Solved! Go to Solution.
2025-06-16 4:51 AM - edited 2025-06-16 4:58 AM
Thanks a lot for the offer!
I found the solution to my problem, but you might incorporate it into future updates of the STM Extension. When using STM32Cube clangd, there is a setting in settings.json (that is auto generated by the extension I assume):
"--query-driver=${env:CUBE_BUNDLE_PATH}/gnu-tools-for-stm32/13.3.1+st.8/bin/arm-none-eabi-gcc"This seems to be the reason for the error messages.
When I change that option to ".../arm-none-eabi-g++" my project didn't display any error messages anymore and clangd recognizes the C++ libraries.
And it seems like the STM32 extension changes that setting back to gcc each time I open my project... so would be nice to change that behavior.
2025-06-16 12:53 AM
Hi @JanusAudio
If there is no confidential aspect n your project could you please share it by message we will help you transforming it to a C++ project.
2025-06-16 4:51 AM - edited 2025-06-16 4:58 AM
Thanks a lot for the offer!
I found the solution to my problem, but you might incorporate it into future updates of the STM Extension. When using STM32Cube clangd, there is a setting in settings.json (that is auto generated by the extension I assume):
"--query-driver=${env:CUBE_BUNDLE_PATH}/gnu-tools-for-stm32/13.3.1+st.8/bin/arm-none-eabi-gcc"This seems to be the reason for the error messages.
When I change that option to ".../arm-none-eabi-g++" my project didn't display any error messages anymore and clangd recognizes the C++ libraries.
And it seems like the STM32 extension changes that setting back to gcc each time I open my project... so would be nice to change that behavior.
2025-06-19 8:20 AM
I was having this issue as well while working on a TouchGFX CMake project in VSCode, which uses C as well as C++ for TouchGFX. Lots of language errors and problems finding headers like assert.h.
My solution was to disable the STM32 clang extension and just use the C/C++ intellisense and that works fine.
I did try the solution above but it will only solve some issues. I was able to fix all the problems by having both gcc and g++ for the query-driver setting.
"stm32cube-ide-clangd.arguments": [
"starm-clangd",
"--compile-commands-dir=${workspaceFolder}/build/Debug",
"--header-insertion=never",
"--clang-tidy",
"--clang-tidy-checks=-*,clang-diagnostic-undeclared-var-use",
"--query-driver=${env:CUBE_BUNDLE_PATH}/gnu-tools-for-stm32/13.3.1+st.8/bin/arm-none-eabi-g++.exe",
"--query-driver=${env:CUBE_BUNDLE_PATH}/gnu-tools-for-stm32/13.3.1+st.8/bin/arm-none-eabi-gcc.exe"
],
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.