2022-08-21 10:35 AM
Hello Community,
I'm a newly user and have a custom PCB.
Now with having set up the Cube IDE I'm struggling that I can't compile just the code like it came out of the CubeMX's code generator.
Can you give me a hint to start?
I already set the compilers optimization for size and varied the min heap and min stack variables, but no improvement.
If the code really is too big, is there any option how to reduce it's size in CubeMX?
Best regards,
Hannes
2022-08-21 1:52 PM
Yes, 16KB FLASH is pretty tight.
I'm building HAL based code into them.
Watch for the floating point library.
Check for initialized memory, if things are constant make sure they like in FLASH, and not both FLASH and RAM
Trick might be to tell linker it has more resources, so it can get closure on what you're trying to build,and then figure out whose eating all the memory resources via the .MAP file
2022-08-21 10:19 PM
As said Clive, this stm32 flavor is tight in memories. Maybe the stack size needs to be optimized. The map file wilk tell you the memory cost of each object file to know where to optimize. If your code needs compiler optimisation to fit, debug witg breakpoints will be painful down the road....
For ram l, " union " is your friend....
2022-08-23 8:15 AM
Hello @Johannes Hofmann
I advise you to check first the memory detail in the Build Analyzer.
Also you can try using the LL library.
Finally if it is possible could you send me the IOC file or the project for further analysis.
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-30 6:49 AM
Hello @Johannes Hofmann
Did the previous replies helped to resolve the issue?
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.