2022-08-14 11:19 PM
hi
after uninstalling:
"en.st-stm32cubeide_1.9.0_12015_20220302_0855_x86_64.exe_v1.9.0"
"en.stm32cubemx-win_v6-5-0_v6.5.0"
"en.stm32cubeprg-win64_v2-10-0_v2.10.0"
and installing:
"en.stm32cubemx-win_v6-6-1"
"en.stm32cubeprg-win64_v2-11-0"
"en.st-stm32cubeide_1.10.1_12716_20220707_0928_x86_64.exe"
in stm32cubeIDE any time push "ctrl+space" for autocomplete, working but after delay for 20 second ! :o
and into 20 second, stm32cubeIDE is hang.
example:
"uint8" now press ctrl+space and after 20 seconds it will show uint8_t and other words...
please help me
---
my pc information:
Processor: Intel(R) Core(TM) i7-7700K CPU
RAM: 16GB
System type 64-bit operating system, x64-based processor
Graphic card: NVIDIA GeForce GTX 1060 6GB
2022-08-16 2:44 AM
Hi @kshin.11 ,
I have the same Environment Cube as you but I don't have this problem, can you see in your Task Manager, if your Pc is not running other programs, which can explain this delay? Do you always have the same problem when you restart your PC?
Regards ,
Diane
2022-08-17 5:30 AM
Hello @kshin.11
Try to create a new workspace. If issue resolved you should try to delete the .pdom files under the work space repo %(workspace)\.metadata\.plugins\org.eclipse.cdt.core\*.pdom
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-30 6:34 AM
Hello @kshin.11
Do you still have the delay issue with the CubeIDE tool?
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.