2019-02-06 3:41 AM
Hi everyone.
Up to now i have been programming STM32 mcus at register level but i have to use cube mx now. So i created a cube mx project only to see if timer 2 works fine. When i build without any problems and run the code on my F303RE board and pause i see program pointer shows at the least function call before while(1) loop which in here is "HAL_TIM_PWM_Start" function. I didn't understand why this problem occured. Can anyone please help me? Below is my simple code. Thank you.
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim2;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_TIM2_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_Base_Start(&htim2);
HAL_TIM_Base_Start(&htim2);
HAL_TIM_PWM_Start(&htim2, HAL_TIM_ACTIVE_CHANNEL_1);
HAL_TIM_PWM_Start(&htim2, HAL_TIM_ACTIVE_CHANNEL_2);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while(1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
2019-02-06 5:05 AM
Going to have to debug it an understand why/where it stopped.
Check it is not in ErrorHandler() or HardFault_Handler()
Check it is not in Default_Handler() due to lack of interrupt handler for things you have enabled.
2019-02-06 5:10 AM
Than you for your answer @Community member. When i looked at disassembly to find where the program really is, i realized that it actually works in while(1), but in the C code window it shows the last function above while(1).
2019-02-06 5:42 AM
Most likely you have optimization flags set. Compiler code optimizations and C level line-by-line debugging are pretty much incompatible.
2019-02-06 5:49 AM
Yes @After Forever , i had made some changes in optimization settings on TrueStudio. After i load the default settings it worked.
Thank you for your answer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.