STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Is there an elegant way of using CubeMX to generate code for two very different configurations in the same program?

The program is alternating between two modes, one is high performance and the second is low power. For perfomance mode the ADC is used with a timer triggering and DMA+interrupt at fast rate. In the low power mode it is intended to make a single conve...

Program does not enter while(1) loop

Hi everyone.Up to now i have been programming STM32 mcus at register level but i have to use cube mx now. So i created a cube mx project only to see if timer 2 works fine. When i build without any problems and run the code on my F303RE board and paus...

N ORhan by Associate III
  • 3263 Views
  • 4 replies
  • 0 kudos

Resolved! Using multiple tasks in FreeRTOS

I am having a strange problem with FreeRTOS in CubeMX, I cannot get multiple tasks to work concurrently. I use the following procedure -Pre: Check STM32Cube_FW is fresh   (v1.9.0 used)Open STM32Cube V1.0   (v5.0.0 used)New Project -> 'Access To MCU S...

Justin1 by Senior
  • 2053 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F4 COMPOSITE implementation

Hi,i am trying to implement my mcu (stm32f407IG) as a composite device with USB FS. I want to use CDC+HID or more how can i implement that with CubeMX ?Are there any examples about that?Thanks for your help.

arduo by Senior
  • 1009 Views
  • 1 replies
  • 1 kudos

Resolved! OCTOSPI - wrong code generation? Bug should be fixed.

Hello, I am debugging a board which contains the MCU - STM32L4R7VI6 and an HYPERRAM IC connected to the OCTOSPI2 port on the MCU. While generating code on the STM32CUBEMX the tool generates the following code snippet at the bottom of the OCTOSPI_INIT...

CesarH by Associate
  • 2044 Views
  • 3 replies
  • 0 kudos

Where is the code generator gone?

Hello!I have upgraded to version 5. Can anybody tell me where the generator command is gone? It used to be directly in one of the 3 menus as far as I remember, something like generate code or something like that.Thanks!K

KY by Associate II
  • 1757 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.