2019-11-12 7:06 AM
I am trying this ADC configuration created by STM32CubeMX
'''''''''''''''''''''''''''''''''''
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = DISABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T2_TRGO;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC1_Init 2 */
/* USER CODE END ADC1_Init 2 */
}
'''''''''''''''''''''''
Parameter
ADC_CLOCK_SYNC_PCLK_DIV2
is grey out in CubeMX and cannot be selected. Only
ADC_CLOCK_SYNC_PCLK_DIV4 and above can be selected.
The effect of this is that I only get 1.4Ms/s conversion if I use this.
If I use ADC_CLOCK_SYNC_PCLK_DIV2 then I can get 2.8Ms/s conversion.
I am clocking the board at 168MHz.
My question is this a problem with CubeMX and if not what can be done to achieve the higher ADC conversion without hacking the code generated by CubeMX
2019-11-12 7:57 AM
I had a look at the data sheet and I think I found the answer.
According to the datasheet ADC maximum clock is typ 30MHz and max 36MHz.
My ARB2 clock is 84MHz which when divided by ADC_CLOCK_SYNC_PCLK_DIV2 will generate a 42MHz ADC clock which is more then 30 MHz, hence CubeMX is correct to only allow ADC_CLOCK_SYNC_PCLK_DIV4 or more.
I guess I am overclocking in my code, the ADC seem to accept 42MHz as the results are OK.
2019-11-12 8:47 AM
> I guess I am overclocking in my code, the ADC seem to accept 42MHz as the results are OK.
As with any overclocking, it may "work". The DS gives you the guaranteed values - if you overclock, it may fail unexpectedly under various conditions.
The best story I have for this was, when on a local forum somebody complained that his AVR program works perfectly except unexpected failure in one particular function. I worked him through some exercises which narrowed down the failure to an address which was on a 0x1000 boundary; only after further extensive querying he admitted he is overclocking the mcu by some 50%...
JW
2019-11-12 10:19 AM
I dropped the main clock from 168MHz to 144MHz and now I can choose ADC_CLOCK_SYNC_PCLK_DIV2 in CubeMX which now generates ADC clock speed of 36MHz. I can now push the ADC to sample at 2.4Ms/s as per DS.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.