STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Not running NAND FLASH with STM32H70VB

Hi,I have a Project which is about data transfering and storaging. I use STM32H750VB micro processor, MT29F32G08CBADBWP-12IT:D Nand Flash and LAN8742A Ethernet Chip for my application. I configure and run Ethernet, ADC, I/O, UART etc. functions with ...

by Not applicable
  • 1137 Views
  • 1 replies
  • 0 kudos

Bug Sys Debug disable on MX_Cube_5.4

Hello, After update the CubeMX from 5.3 to 5.4, and I change the IOC and generate a new code, a error appear and debug is disconnected. Before the update:After the update:I doesnt change nothing in the code, just change a GPIO_Input to Output.I insta...

0690X00000ArnWqQAJ.jpg 0690X00000ArnX0QAJ.jpg
joaoleao by Associate II
  • 653 Views
  • 0 replies
  • 0 kudos

Where to report bugs in the STM32CubeMX?

It seems the clock configuration is not generated correctly by the Cube.Used STM32CubeMX Version 5.2.1 for STM32G070RBT deviceThe root cause seems to be the RCC_CCIPR_TIM1SEL is not defined.As a consequence the RCC_PERIPHCLK_TIM1 is not available and...

Andi by Associate III
  • 1724 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.