2020-05-28 9:12 AM
And I can only click on pins to select function but no clicking of left side list items makes me unable to set HSE resonator.
What is wrong?
2020-05-28 9:28 AM
You need to enable the HSE before you can select it.
RCC -> HSE -> Crystal/Ceramic Resonator (or whatever)
2020-05-28 9:38 AM
Thanks for prompt response.
However the issue is when I click RCC nothing happens. No detail panel where I can change from disabled to resonator.
Both CubeIDE and CubeMX is then unusable on my IMac.
I have installed cubeMX on company windows laptop - win version is OK. But I can not use this comp for STM32 development. So going back to original Q : is it some java issue, or something else?
2020-05-28 11:00 AM
Just noticed, when I change from pin view mode into the system view, then clicking on objects like RCC opens panels so I can modify them. Similairly to add panel for analog inputs, I must first change some pin to ADC, then in system view clicking ADC1 reveals ADC panel so I can quickly select other pins.
No idea however how to change I2C or USART modes...
2020-06-17 1:07 PM
No help?
Shall I understand that CubeX in not usable on my iMac?
Still no possibility to select check boxes with mouse, click on items to open panels etc...
2021-05-17 2:52 PM
New iMac, Big Sur, fresh install and the same, I can not use CubeMX or CubIDE/Device confgurator on OSX.
I guess it is something with Java but no idea how to fix that.
Example:
I can expand "Timers". I am clicking on TIM1 label -> no action, I can not open additional panel to deal with TIM1 configuration.
As I am unable to do any configuration changes, I can not regenerate code.
What I can only do is to select development board, like Nucleo-F031, and stick to default config,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.