2021-06-22 10:16 PM
I started a STM32 framework project here: https://github.com/FBergemann/STM32-FreeRTOS-Framework/tree/dev-usb-host-msd. And i am currently busy to set up logging to console and USB FS (as Host to USB stick). But i didn't manage to enable USB OTG FS. I think it's due to an error in enable VBUS. Because in https://github.com/FBergemann/STM32-FreeRTOS-Framework/blob/dev-usb-host-msd/USB_HOST/Target/usbh_conf.c there is
#79 GPIO_InitStruct.Pin = USB_VBUS_Pin;
#80 GPIO_InitStruct.Mode = GPIO_MODE_INPUT; /* wrong?! */
#81 GPIO_InitStruct.Pull = GPIO_NOPULL;
#82 HAL_GPIO_Init(USB_VBUS_GPIO_Port, &GPIO_InitStruct);
I followed instructions according http://evenlund.blogspot.com/2016/10/usb-storage-with-stm32f4-discovery-and_58.html
and https://www.youtube.com/watch?v=uIOb5sSFyUY.
Can you please tell me, what i am doing wrong here?
- thanks!
regards,
Frank
Solved! Go to Solution.
2021-07-05 1:55 AM
Hello @FBerg.1,
Unfortunately there is no .ioc file for F4, F7, H7 families .. and the examples/demo provided are developed directly with HAL. May be .ioc files will be available in the Cubes of new coming products.
There is no difference between STM32F769 & STM32F767 devices except the DSI interface which is available on F769.
For the boards, the main difference I think is the clock configuration. So I think you have to configure the board with periph initialization and then follow the example which I pointed out just for reference for USB config, then put your user code..
For the generated erroneous code with CubeMx I will escalate the subject internally, if there is an issue it will be fixed.
STM32
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.