2023-03-08 10:45 AM
I am learning the stm32 using a stm32g070cbt6 micro controller with custom PCB with keil. When I add an external pull-up to the pa4 pin and use it as an input pin. Nevertheless, when I read the pin, the output is low always, even though on the hardware pin is high(3.3v). Yet I couldn't figure out why it happened. Please assist in finding this problem.
Thanks in advance.
#include "main.h"
void SystemClock_Config(void);
uint16_t count =0;
int main(void)
{
HAL_Init();
SystemClock_Config();
RCC->IOPENR |= (1<<0);
GPIOA->MODER &= ~((1<<8) | (1<<9));
while (1)
{
if (!(GPIOA->IDR &(1<<4))) // if the pin is low count should increament
{
count++;
}
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
RCC_OscInitStruct.PLL.PLLN = 9;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV3;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
}
2023-03-08 12:13 PM
The pin is low - see IDR register. Try to declare count as volatile.
2023-03-08 2:11 PM
from what i can understand is that you turn on clock for GPIO and then in just next instruction use GPIO registers. I would try adding something in between just to try.
second
GPIOA->MODER &= ~((1<<8) | (1<<9));
this set up A4 to mode 00 which is input. all fine.
second - how do you check that count as it's infinite loop?
It's not set to volatile - so this loop may increment register, without even touching global variable.
2023-03-08 6:30 PM
That's problem, i add 1k pull up at PA4 which makes this pin high, but actually it is low.
2023-03-08 6:47 PM
@Community member I appreciate your reply.
Purpose for count only:I want the count to increase only when a low pulse is detected at a pin.
The issue is with pin PA4 on port A. On the hardware side, I added a 1K pull-up resistor to make the pin high theoretically, but in practice, I get low. could propose anything
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.