2023-03-17 4:49 AM
2023-03-17 7:02 AM
You will also find some additional information and hints in this thread.
Regards
/Peter
2023-03-17 7:00 AM
Hello @THart.3 ,
Please you mean this AN : Using the hardware real-time clock (RTC) and the tamper management unit (TAMP) with STM32 microcontrollers?
You can check the available examples in the FW for the STM32L476 : STM32Cube_FW_L4_V1.17.2\Projects\NUCLEO-L476RG\Examples
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-17 7:02 AM
You will also find some additional information and hints in this thread.
Regards
/Peter
2023-03-20 12:45 AM
Hi. Thanks for your answer.
Yes there on page 40 is the Smooth calibration example with the Nucleo-L476 and I'm working with this project.
I made a little progress, in the tim.c file they used LSE as clock with following instructions:
TIM2->OR1 = TIM_TIM2_ETR_LSE;
TIM3->CR2 |= TIM_TRGO_OC1REF;
I wrote these in the wrong fuction. Now i just have the problem, that in the TIM2_IRQHandler:
if (__HAL_TIM_GET_FLAG(htim, TIM_FLAG_CC1) != RESET) that it never goes in into this if query, but the interrupt occurs.
regards
2023-03-20 12:46 AM
Hi thank you for your answer.
i already read that thread, its very usefull for understanding.
i just have problems to implement the smooth calibration in my project.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.