2024-09-19 1:46 PM - last edited on 2024-10-01 7:39 AM by Andrew Neil
Hello,
Since the latest release of CubeMX (6.12.1), I have been encountering syntax errors related to the "FLASH.ld" file. This issue only arises when I generate code while setting the Toolchain/IDE to CMake. I am using STM32H753IIKx. It seems that CubeMX does not specify which RAM to use when setting the Toolchain/IDE to CMake.
I have also included the FLASH.ld file that was generated for your reference.
Thanks for your help.
Solved! Go to Solution.
2024-09-29 5:23 PM
In STM32CubeMX, just click on "TOOLS" menu then select both:
Save project and re-generate it. The linker file will be correct
2024-09-29 5:45 PM - edited 2024-09-29 5:51 PM
I WAS WRONG! Sorry ....
The correct action is to select FLASH (or RAM) in "Search an Application Region" :
Then save and re-generate project.
:(
2024-09-30 11:10 AM
Well, this is not the solution either. In my case, for STM32F103C8Tx, CubeMX does not allow configuring it's memories (under tools).
CubeMX produces an .ld file completely different when exporting for Makefiles and exporting with build files for STM32CubeIDE. Strangely, the .ld file produced for using with STM32CubeIDE reports it is generated by STM32CubeIDE and not by MX.
FYI, I am attaching the two different linker files
2024-09-30 12:32 PM
And this prevents rolling back to previous version or CubeMX
2024-10-01 7:04 AM
Hello,
Thanks for the reply. But a quick question. I cannot find "Search an Application Region" in CubeMX.
Can you please tell me where I can find it?
Thanks
2024-10-01 9:18 AM
I believe this present under tools only for some devices. At least for a F103C8Tx it does not exist
2024-10-04 1:35 PM - edited 2024-10-04 1:36 PM
Wow, this is so frustrating. I lost the better part of a day's work due to this bug. Not so much lost code, but lost time, trying to figure out what I'd done wrong in my project. To then finally discover it's not anything I did wrong, but rather it's a bug in CubeMX. Lame.
For anyone experiencing this issue, here's what I did to resume productivity.
The take away is: do frequent git commits, and never trust that letting CubeMX migrate your project isn't going to break something. The irony for me was, I'd updated CubeMX due to a bug in the version I'd been running (fields in the app would suddenly become non-responsive to keyboard input).
2024-10-05 12:16 AM
Another option (but not without risk), you can edit the IOC file and change the mininum cubemx required version, I am pretty sure they did not change anything between 6.12.0 and 6.12.1 they just broke the tool
2024-10-07 2:49 AM
CubeMX forgets about references to RAM
We have:
Should be
And at the end of .data section definition:
Should be:
Also for .bss
Should be:
And for ._user_heap_stack we have:
Should be:
2024-10-19 3:14 AM
When the fixed version will be released
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.