2023-08-08 5:33 AM
Despite referring to the STM32F0 label (can't this forum have a simple one labeled as a general problem for STM32CubeMX???) the problem exists for ALL situations and MCU's where you simply start working with the STM32CubeMX.
Since several years ago, some colleagues on this form (and myself for 1-2 months) continue to report a completely stupid mess in the stm32CubeMX that makes it completely useless (again I attach a picture of today's nonsense and that completely prevented me simply from doing my work at the University - I'm sick of it!) No one at TS has (apparently) spent even a minute trying to solve such a stupid problem. For now (and against my will) I will migrate to NXP MCUs, which at least the configuration software works! As soon as someone at ST fixes the problem (which drags on for years!) please let me know.
2023-12-18 1:08 AM
After years, finally I found a workaround. This issue is really a pain in my ass!!!!!!!
On windows set environment variable J2D_D3D to false can fix this.
You can use the PowerShell command to do this as
setx J2D_D3D false
It seems like unappropriated graphical acceleration issue on windows platform which provide by DirectX3D.
2023-12-18 1:25 AM - edited 2023-12-18 1:35 AM
One more thing to catch up, STM32cubeMX is not only java GUI application mess up on windows system (such as jadx, JD-Gui). So, I think the problem paraphs not directly relate to STM32cubeMX itself. On my opinion "the GUI mess up" things tend to happen when user use text editor widget and drop box selector widget.
There are some useful links which issue the same "mess up" problem:
OpenRocket GUI Glitch | Rocketry Forum - Model Rocketry Forums
[MCL-4485] Launcher GUI glitch after trying to change profile. - Jira (mojang.com)
Graphical glitch in the GUI version Windows 10 - FileBot
add flag to start the app may also a workaround: -Dsun.java2d.d3d=false
2024-02-04 8:32 AM
I have this issue as well, on my machines with RTX 4080 dies in them. This isn't acceptable.
2024-02-04 8:50 AM
You can reproduce it by purchasing a decent video card. Try it on an RTX 4080 with the latest nvidia game drivers, and you'll see it right away.
2024-02-04 8:54 AM
I think it's any decent NVidia GPU. Both my RTX 4080 (laptop says 4090, but it's really a 4080 desktop die) reproduce the problem.
2024-02-09 3:00 PM
Dear All
Apparently good news!
Disabling the use of Direct3D pipeline in Java as indicated by @Vertexi ('setx J2D_D3D false') seems to work (I tested it and managed to work with CubeMX for more than two hours without any problems).
Naturally this is a workaround but for now I think it works. On my desktop I have an Nvidia GTX 1660 Super card. In the next few days I will check how reliable this workaround is.
Best
2024-03-01 12:46 AM
Hi @Luiz Pereira ,
Thanks a lot for the confirmation that it fix your problem. We will perform some regression test in our side and see if this can be added by default when launching the tool so this issue can disappear forever...
----------------------------------------------------------------------------------------------------------------------------------------------------------
To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
2025-02-02 1:11 AM
Hi,
Although the proposed solution may work for windows, on Ubuntu Linux I still see the issue. I am running Ubuntu 24.04.01 LTS on a VMWare virtual machine and I have the same issue.
The problems seems to be in the Java UI hardware acceleration. With the help of chatgpt I tried couple improvements and the following one seems to fix the issue in Ubuntu and it's reproducible -> force software rendering
export _JAVA_OPTIONS='-Dsun.java2d.opengl=false -Dsun.java2d.xrender=false'
./STM32CubeMX
The interface might be a bit slow, but it works. As soon as you open a new shell and start STM32CubeMX without this java option, then the problem appears again.
2025-02-17 1:16 PM
This has been the worst piece of software I've ever used for years. ST just can't get it to work properly. There's always some issue with a chip. If one issue is fixed, another one pops up somewhere else. It's just embarrassing how poorly it works.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.