2017-12-08 12:56 PM
After CubeMX griped that my software was too old, I tried to upgrade from the New Libraries Manager, but there was an error downloading the file. I fetched the file manually, then tried installing using the New Libraries Manager 'local' function. I get a 'Problem during unzip of file', though the file unzips fine under 7Zip.
Can anybody provide an alternate method of installing this library? This is preventing me from even _starting_ a project.
#cubemx-zip-file-new-library-managerSolved! Go to Solution.
2017-12-13 1:44 PM
Hmmm. That might be the trick. At least running as Admin - it's still running, v. erroring our after a second. The unzip appears to be glacial, but it continues.
And it finally finished. This appears to the 'the answer'.
Thanks very much
2017-12-08 1:47 PM
This is my share of L4 V1.10.0
https://drive.google.com/open?id=0B7OY5pub_GfIZVVxcGhJVGR4SnM
Make sure you have enough free space on you drive to hold the 2GB and the ~4GB, or whatever, it takes unpacked. Delete older stuff from the repository if necessary.
The software doesn't test for available space, so you can get non-specific errors about downloads or unpacking steps when the drive fills up. Run into issues on a couple of older machines with smaller hard drives, and having downloaded multiple libraries from multiple families.
2017-12-13 11:15 AM
Very good hint, but with 67GB free, I don't think that's the problem. Thanks for sharing the file. I will see whether it installs.
I checked the file's integrity by unzipping it (Windows native tool. not 7-Zip), then attempted, without success, to install it using the 'local' button in the CubeMX dialog.
Grrrr...2017-12-13 1:30 PM
And you have v4.23.0 of CubeMX?
AV software? Run 'As Administrator' ?
For someone at ST to troubleshoot this you will likely need to provide more detail about your specific setup, version of Windows, other softwares, etc.
2017-12-13 1:44 PM
Hmmm. That might be the trick. At least running as Admin - it's still running, v. erroring our after a second. The unzip appears to be glacial, but it continues.
And it finally finished. This appears to the 'the answer'.
Thanks very much
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.